Issue
The XIF parser could fail if there is a "-sign in a commented row in the XIF default field.
Environment
TAC Vista
Cause
The XIF parser could fail if there is a "-sign in a commented row in the XIF default data field.
Example:
# -----------------------------------------------------
# -----------------------------------------------------
FILE value 1 1
##dde1 "1,2,3\x00,1,2;" // UCPTdownDriveTime SNVT_time_sec
0x66,0x66
##dde3 "1,2,23x00,2,2;" // UCPTupDriveTime SNVT_time_sec
Resolution
Just removing the "-sign will work:
# -----------------------------------------------------
# -----------------------------------------------------
FILE value 1 1
##dde1 1,2,3\x00,1,2; // UCPTdownDriveTime SNVT_time_sec
0x66,0x66
##dde3 1,2,23x00,2,2; // UCPTupDriveTime SNVT_time_sec