Issue
Filtering The AnalogSamples_xi.rpt SevenReport using the cell definition
Environment
I/NET Seven Reports
Cause
In some cases, the cell number can be used on a 7 trend to allow only trends of a certain type to show up in reports. If this rule is applied, you will need to change the stock reports to allow for this function.
Resolution
- Open the AnalogSamples_xi.rpt file in Seven Reports
- Cancel the Date Time range selector
- In the Design View, click on the second icon from the left, directly underneath the word "Design" the tool tip labels it as "Select records to be used in report Select Expert"
-
Click on the "
" tab - browse to the bottom and expand "RptTrendDefinitions"
- Click on "CellNumber"
- Click OK
- In the left hand drop down select "is equal to"
- In the Right hand drop down, enter the cell number you wish to filter for.
- Click OK
- Preview the Report
- Save it using a different file name.