Issue
The MnFlow shadow device, in Niagara R2, comes with six objects. What do the inputs and outputs cross-reference to down in the Micronet 2000 VAV controller?
Environment
Niagara R2 (ASD driver)
Micronet 2000
Cause
Programming Niagara objects to control setpoints in the Micronet VAV
Resolution
Document F-25720 lists tables illustrating what each input and output is mapped to in the Micronet VAV.
MnFloEmsDi object in Niagara R2:
MnFloEmsAi object in Niagara R2:
MnFloDvOuts & MnFloAvOuts objects in Niagara R2: