Issue
How to program software for Automatic Windows
Environment
BAS
SIGMA
Cause
Windows are open and close type, but the requirement is for the Windows to modulate.
Resolution
The windows can be modulated but only in fixed stages.
The window travel time needs to be known from fully closed to fully open and vice-versa. Open and close should be equal time.
The example below is for automatic windows in a classroom where the teacher could override the windows open or closed, along with the other interlocks e.g. wind direction and rain.
Click here for the word document or here for the pdf containing the objects that are required to achieve this.