The SEQROT object in the Network8000 integration in the AS seems to work with constant input values but not reference pointers.

Issue

The SEQROT object in the Network8000 integration in the AS seems to work with constant input values but not reference pointers.

Product Line

SmartStruxure Solution

Environment

AS version 1.3.0 & 1.3.0 SP1 with Network8000 interface

Cause

After the object has been defined to use constant inputs those input values must be reset to Null before the reference inputs will be used.

Resolution

The Analog input constant can be returned to Null by highlighting the value it contains and clicking the delete key.  The field will be empty until a save is done.  With a digital input such as the Rotate stages constant simply highlight the value and click the delete key and it will change to Null.