Supported Version of Windows Server and SQL Server for StruxureWare Reports Server

Issue

Supported Version of Windows Server and SQL Server for StruxureWare Reports Server

Product Line

SmartStruxure Solution

Environment

Reports Server

Cause

Reports Server is only supported on a specific operating systems and SQL Server versions.

Resolution

SmartStruxure 1.4.1 and below - Datasheet

Windows Environment:

  • Microsoft Windows Server 2008 R2 (64-bit)

SQL Software Options

 

SmartStruxure 1.5 and above - Datasheet

Windows Environment:

  • Microsoft Windows Server 2008 R2 (64-bit)
  • Microsoft Windows Server 2012 (64-bit)
  • Microsoft Windows Server 2012 R2 (64-bit)

SQL Software Options