Some documentation seems to indicate that the serial port on the NPR can talk at 9600. Can it?

Issue

Some documentation seems to indicate that the serial port on the NPR can talk at 9600. Can it?

Product Line

TAC I/NET

Environment

NPR 2000

Cause

Configuration Question

Resolution

No. The port can be configured for 19,200 only.