Issue
An error message indicates that EPICLM.exe can't be found in data1.cab using the Epi integration for badging or a 1309 when installing Cyberstation
Product Line
Andover Continuum
Environment
- Windows XP
- Windows 7
- Windows Server 2003
- Windows Server 2008
Cause
Kaspersky Anti virus is identifying and removing the file from the data1.cab during a scan.
Resolution
Place the cab file or the EPICLM.exe as an exclusion in Kaspersky's or EST NOD32 scan. For additional information see Kaspersky's website.
http://support.kaspersky.com/4084
Note: The data1.cab file may need to be restored from the original CD or Continuum install zip file and then uninstall/reinstall EpiBuilder with the exclusion list in place to repair the problem. See Uninstalling and reinstalling EpiBuilder or error opening EpiDesigner configuration database for more information.