Personnel Import Utility documentation

Issue

There's a need for information on the Personnel Import Utility

Product Line

Andover Continuum

Environment

Continuum

Windows XP

Windows 7

Windows Server 2003

Windows Server 2008

Cause

Finding the information on the Personnel Import Utility may be difficult to find, this LL makes it easier to locate.

Resolution

The information for the Personnel Import Utility can be found in the latter part of Chapter 19 on Personnel.

There is additional information in Appendix C related to the tables and XSLT file

To download a copy of just the PIU manual click here