What is the correct cable to use to communicate with the NPR 2000 via its serial port

Issue

What is the correct cable to use to communicate with the NPR 2000 via its serial port?

Product Line

TAC I/NET

Environment

I/NET Site

Cause

What is the correct cable to use to communicate with the NPR 2000 via its serial port?

Resolution

The getting Started book incorrectly specifies that you may connect the com port of the computer to the com port of the NPR 2000 using a standard serial cable. The correct cables are the same cables used to connect to a 77xx01 emutap, the CBL072. Article 5588 has more information on this cable.