Getting javax.baja.xml.XException: Error parsing value error message when attempting to add a new driver network to the I/A Series G3 station's Drivers container.

Issue

Getting javax.baja.xml.XException: Error parsing value error message when attempting to add a new driver network to the I/A Series G3 station's Drivers container.

Drag and Drop - drag network container from palette and drop onto the Drivers container

Copy and Paste - copy network container from palette and paste into the Drivers container

Drivers Manager (New selection) - wizard to add new driver

Error details displayed:  com.tridium.fox.session.ServerException: javax.baja.xml.XException: Error parsing value [38:4]

Product Line

TAC I/A Series

Environment

Enterprise Network Server, ENS, ENC, JACE

Cause

The module associated with the driver has not been installed in the local modules folder or remote station.

Resolution

Enterprise Network Server

  1. Stop Workbench
  2. Copy the missing module directly into ~\modules directory for the version of I/A Series G3 being used.
  3. Restart Workbench

ENC or JACE

  1. Open the platform for the ENC/JACE
  2. Install the module using the Software Manager.
  3. A station reboot may be required.