Unable to find Part number for a ATV 21 Variable Speed Drive

Issue

I'm looking for a part number for the ATV 21 Variable Speed Drive but it does not appear on the part number list

Product Line

Field Devices, Pelco Transmission & Power

Environment

ATV 21

ATV 212

Altivar 

Variable Speed Drive

Cause

Part number has been discontinued

Resolution

There is now a new name for the ATV 21 Variable Speed Drive as this old version has now been updated

The new name for the ATV 21 is ATV 212 or Altivar 212

the below is a link to the Schneider Electric web site where all documentation, part numbers, distributors and Support can be found

Altivar 212