If the Filemaster workstation is powered off, file equalization will not occur

Issue

If the Filemaster workstation is powered off, will file equalization still occur?

Product Line

TAC I/NET

Environment

I/NET file equalization

Cause

The filemaster is required for equalization.

Resolution

If the filemaster workstation is powered off, or if EqualSrv is not  available, file equalization cannot occur. Furthermore, other host  workstations will not be able to modify any of the equalized files. It is recommended that the filemaster workstation be powered by a uninterruptable power supply (UPS).

See TCON 209, 1-13 for more information.