Is there a repeater available for a MN-Sx cable run that goes beyond the specified distance?

Issue

A MN-Sx sensor is installed more than 200 feet away (the maximum specified) from a MNL controller.
The dynamic temperature value drops in and out at the controller.  Is there a repeater that can be installed to improve communications?

Product Line

TAC I/A Series

Environment

MNL

MN-Sx

Cause

Cable run extends beyond the specified 200 feet.

Resolution

There is no repeater available that can be used for the MN-Sx cable run.