Can I assign an IP address to each NPR after I place it on the network?

Issue

Can I assign an IP address to each NPR after I place it on the network?

Product Line

TAC I/NET

Environment

I/NET site

Cause

Can I assign an IP address to each NPR after I place it on the network?

Resolution

No. A unique IP address must be entered for each NPR before it is connected to the commercial network. (TCON209 2-27)