Issue
After Click "Time Zoom in" from the pop-up menu when right click the chart in group, the trend chart maybe fill out the screen, because there is no scroll bar for time scale, it is hardly to move the chart to the right time period for viewing.
Environment
Continuum 1.81~1.94
Windows XP
Windows 7
Group
Cause
There is no scroll bar on the chart, it is hardly to move the chart to the right time period for viewing.
Resolution
Left-click the time scale bar at the bottom of the chart, and hold the left mouse button, then move to left or right until the desired time period.