What is the limit to the number of objects that can be created in a Workstation?

Issue

What is the limit to the number of objects that can be created in a Workstation?

Product Line

Andover Continuum

Environment

Continuum Cyberstation

Cause

Want to create a large number of AnalogValue's and BinaryValues in the Workstation for programming and display purposes.

Resolution

There are no limits to the number of variable objects that can be created in the Workstation. There may well be some practical limits based on the SQL limitations but for all intents and  purposes this limit will most likely not be reached on a full SQL install. You may have issues with DB size on an SQL Express system but even then, the AV / BV objects don't actually take up that much physical space.

As an example, I've tested this on my v1.94 system and have been able to create over 2500 AV's in my Workstation folder without any issues.