Issue
Why do the default Continuum Menu pages not look "sharp" on very high resolution monitors?
Environment
Cyberstation V1.94
Cause
Only one set of default .bmp menu screens are provided with a Cyberstation install.
Resolution
The default menu pages supplied in a Cyberstation V1.94 SP1 installation are bitmaps of 1020 x 662 resolution.
If you are using a very high resolution monitor with a much higher resolution you may want to re-draw these example menu pages to suit the sites requirements.