Creating a Counter input in b3 controllers.

Issue

b3 controllers in StruxureWare Building Operation do not seem to support Counter inputs.

Product Line

SmartStruxure Solution

Environment

  • Counter Inputs
  • b3

Cause

SmartStruxure does support the creation of Counter inputs within b3 controllers.

Resolution

Counter inputs are Analog Inputs.  When the Object Creation wizard is used to create an Analog input the user is prompted to select the electric type.  At this point select Counter.