XBuilder crashes on Windows 7 32-bit computers

Issue

XBuilder crashes when opening a project or simply opening the editor

Product Line

TAC Vista

Environment

  • TAC Vista 5.1.8 and earlier
  • Windows 7 32-bit computers

Cause

Due to some Windows issue, XBuilder may crash on SOME Windows 7 32-bit computers.

Resolution

This issue is solved in TAC Vista 5.1.9.

For earlier version hotfixes, please contact local product support.