Is it possible to use Sysman alert server with StruxureWare Building Operation?

Issue

Is it possible to use Sysman alert server with StruxureWare Building Operation? 

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation 1.X

Cause

Customers may wish to send important alarms to duty staff via SMS. Sysman alert server is one way of doing this and is easy to configure.

Resolution

This is possible. The following document details the setup procedure: Sysman alert server with StruxureWare Building Operation

More information can be found on Sysman's website.

Part Numbers:

1. SysManSMS ALERT SERVER: 900800600

2. SysManSMS GSM Modem: 900800610

 

In the UK when ordering please use the below part numbers.

1. SysManSMS ALERT SERVER: 802000

2. SysManSMS GSM Modem: 100002