Error 0x00001402 (Reached end of the list).

Issue

A Plain English program is becoming disabled.  The controller error log logs the following error.

0x01402 (Reached end of the list).

Product Line

Andover Continuum, SmartStruxure Solution

Environment

Continuum

Plain English

Error

b3

i2

Cause

0x00001402 (Reached end of the list) is a Plain English error.  This error most often occurs when a program is calling a Plain English Function that contains no byte code..

Resolution

Edit each InfinityFunction in the controller to determine which function is empty (contains no programming).