Issue
Is it possible to acknowledge an alarm from a TGML graphic?
Product Line
SmartStruxure Solution
Environment
TGML graphics in StruxureWare Building Operation workstation and webstation.
Cause
Customers may wish to simplify the user interface and have a TGML graphic as the interface for all user operations.
Resolution
It is not possible to bind to an "acknowledge" attribute of an alarm from TGML, as this is not exposed. Our recommendation would be to use a panel and have an alarm pane in the panel as well as the graphic.