How many points per driver can an Enterprise Network Server (ENS) be licensed for?

Issue

How many points per driver can an Enterprise Network Server (ENS) be licensed for?

Product Line

TAC I/A Series

Environment

I/A Series G3 ENS Drivers

  • ENS-BAC-NET
  • ENS-BAC-CL
  • ENS-MOD
  • ENS-MOD-SL
  • ENS-OPC
  • ENS-SNMP

Cause

Each of the ENS base drivers includes support for 500 points. Additional blocks of 500 points each can be added to the license. 

Resolution

In terms of licensing, there isn't a limit to the number of points each driver can be licensed for. However, the actual number of points used will be dependent on the computer's resources (CPU, memory etc.).