Issue
How many events can be saved in the Enterprise server version 1.4.1?
Product Line
SmartStruxure Solution
Environment
StruxureWare 1.4.1.
Cause
The number of events which could be saved in 1.4.0 was 200 000 which some customers have thought is too few.
Resolution
The number of events which can be saved in the ES version 1.4.1 is increased to 1,5 million.