Is there a problem with special days in time schedule operations?

Issue

Is there a problem with special days in time schedule operations?

Product Line

TAC I/NET

Environment

I/NET Site

Cause

Is there a problem with special days in time schedule operations?

Resolution

No, the problem most often is in programming. Our software operates such that if there is a special day defined, anywhere in the system, all other time schedules are affected. If they have no entry for that special day, they will do NOTHING. Therefore, if a person defines a special day in one schedule, they must visit all others and define what they are to do on that day also. If it is an access control system, this applies to both door mode and personnel schedules. Read the release announcement for I/NET 2.44a.