MBus to Modbus TCP

Issue

MBus to Modbus TCP

Product Line

TAC Vista, Andover Continuum, Satchwell Sigma, SmartStruxure Solution

Environment

Mbus

Modbus

Cause

How to read MBus devices into a BMS System using Modbus TCP

Resolution

There are different methods, but these are generally using a Modbus RTU / Mbus gateway and then converting it to Modbus TCP. The following ADFweb solution allows Mbus to be read directly into a Modbus TCP device.

Click here for the datasheet.