Showing all points in the StruxureWare Database.

Issue

Showing all points in the StruxureWare Database.

Product Line

SmartStruxure Solution

Environment

Enterprise Server

Automation Server

Cause

In some instances you may need a complete list of I/O or values on a site.

Resolution

This process will show you the majority of objects on the system. It is possible that some will not be listed.

  1. For EACH Server on the system.
  2. In the System Tree Pane, expand the System Folder
  3. Expand to the Modules/RuntimeDBManager/VariableManager folder
  4. Click on the Variables Folder
  5. Copy the Contents to an Excel Document and repeat for each AS on the system.