What type of BIN is used when selecting Typical or the default install of I/NET 2000?

Issue

What type of BIN is used when selecting “Typical” or the default install of I/NET 2000?

Product Line

TAC I/NET

Environment

I/NET 2000 site

Cause

Refer to the Communication chapter in TCON209, I/NET 2000 Technical Reference Guide for information on synchronous versus asynchronous communication.

Resolution

Determine whether you will use synchronous or asynchronous communication. Setup's Typical option (the default) installs asynchronous BIN files. You should choose the Synchronous option to install synchronous BIN files. You may switch from synchronous to asynchronous, or vice versa, at a later date by choosing the Custom option and then selecting the appropriate controller binary files. Instructions are provided in Chapter 2, Installing I/NET in TCON 213.