Pictures of former TAC and Schneider Electric Controller(s) & Devices

Issue

What does that controller/device look like

Product Line

TAC I/NET, TAC Vista, Andover Continuum, Satchwell MicroNet, Satchwell Sigma, TAC I/A Series, Field Devices, SmartStruxure Solution, SmartStruxure Lite

Environment

Site with TAC or Schneider Electric Controller(s)

Cause

Questions concerning what a controller looks like, or if there are no labels on the controller which help identify.

Are photographs or drawings available?

(This is an article in progress. Have one that is not listed? Please help by taking a good picture(s) and including or send to Product Support)

Resolution

I/NET:
7728
7728 Left side
7728 Right side 
7790
7790 side
7790 older model 
7790 older model side 
7798C Top
7716
7920
7920 side 
MR-AHU
MR-AHU left side
MR-AHU right side
P8UI8DO Expansion board 
SCU1284
SCU1284 side

Continuum:
ACX5720
ACX5720 Open
CX9702 
b4920
b4920 Open
BCX1
BCX1 open
i2-600 Series
i2.600 Series Open 
i2_850
i2_850_Open
i2_887_L_115 
i2_920
i2_920_open
CX9400 with three 32s and two 16s in 8 card rack
CX9400 CPU front

CAD Drawings for the Continuum controllers are also available on The Exchange Download Center: Link Here.