I/NET Access Control work with retina, palm or fingerprint readers

Issue

Will I/NET access control work with retina, palm or fingerprint readers?

Product Line

TAC I/NET

Environment

I/NET 2000

I/NET Seven

Cause

Will I/NET access control work with retina, palm or fingerprint readers?

Resolution

Yes, provided they send a data string of the supported Wiegand bit rate for the version and firmware of I/NET in use, and it is in the order we expect. Refer to Lessons Learned Article #2887 for an example or contact Product Support for more details.