Xenta SMTP Port number will not change.

Issue

When using a web browser to change the SMTP port number from 25 to, for example 465, and save, if leaving the page and navigate back to that page, the changed port number reverts back to 25.

Product Line

TAC Vista, Satchwell MicroNet

Environment

Xenta 555

Cause

When using a web browser to change the SMTP port number from 25 to, for example 465, and save, if leaving the page and navigate back to that page, the changed port number reverts back to 25. 

Resolution

Change the port number to something other than 25 in the Xbuilder project then upload the Xenta's project again.

For example:
From.

 

To:


Now, in the future, you will be able to change the SMTP port number using a browser, if changes are required.