Niagara G3 Serial Tunnel to Microsmart > correction in the Installation and Configuration Guide (F-27523).

Issue

Niagara G3 Serial Tunnel to Microsmart > correction in the Installation and Configuration Guide (F-27523).

Product Line

TAC I/A Series

Environment

Niagara G3

MicroSmart Driver

Cause

A documentation error

Resolution

A serial tunnel is included with the MicroSmart Network (see below):

There is no need to add a SerialTunnel to the station as illustrated in the manual on page 22:

The TunnelService is still required in the Services folder.