Computer will not recognize NIC709-USB

Issue

When trying to install a NIC709-USB the computer will not recognize it.

Product Line

TAC Vista

Environment

  • Vista
  • LonMaker
  • NL220
  • Windows 7 64-bit
  • Windows 2008 Server 64-bit

Cause

A NIC709-USB will not work with a 64-bit OS.

Resolution

If you have a 64-bit OS then you must use a NIC709-USB100 instead of a NIC709-USB.