Issue
Some security software will report that there are vulnerabilities for SSL of Xenta Server. Some vulnerabilities look like:
- SSL Server allow anonymous authentication vulnerability
- SSL Server allow Cleartext communication vulnerability
- Weak encryption model
Product Line
TAC I/NET, TAC Vista
Environment
Vista
I/NET
Cause
This is how Xenta Server designed to work.
Resolution
There is a security enhancement for Xenta Server in Xenta 5.1.9. Update the firmware to Xenta 5.1.9 will fix these vulnerabilities. You can download Xenta 5.1.9 from Buildings Download Center.