What is the limit of nodes on a segment?

Issue

What is the limit of nodes on a segment?

Product Line

TAC I/NET

Environment

I/NET Site

Cause

What is the limit of nodes on a segment?

Resolution

There can be up to 64 nodes in a segment under optimal conditions(FTT-10A and TP/XF-1250) or 128 (LPT-10). Two segments can be connected by the use of a repeater, but are still one channel.