Issue
When using the optional expansion enclosure within the 7780, is there a longer length matrix cable available than the standard 6-foot cable?
Environment
I/NET Site
Cause
When using the optional expansion enclosure within the 7780, is there a longer length matrix cable available than the standard 6-foot cable
Resolution
There is no alternative to the 72-inch matrix card ribbon cable (part# 606105-0041) that we supply. Since these signals are low voltage levels and there is no shielding within a ribbon cable, the 6-foot distance cannot be exceeded.