Zoom feature is lost when a windows control is added to Pinpoint


In Design mode, you can view and then zoom in and then out, but once a windows control is added, the zoom feature is lost

Product Line

Andover Continuum




Windows XP

Windows 7

Windows Server 2003

Windows Server 2008


Functions as designed


FAD - Functions as designed. This issue was detected and written up and investigated by engineering. Based on the engineer that wrote Pinpoint, it was decided to not make this feature available with Windows control added. We know zoom works in Design mode until you add the Windows Control, but the coding required to make it work with the Windows Control would have been too much and cause instability. Engineering decided to make that feature unavailable.