Assigning an Extended Trend Log to a Meter Object

Issue

Assigning an Extended Trend Log to a Meter Object

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation Reports Server

Cause

User wishes Meter Logs to show up in Energy Reports

Resolution

  1. Configure the Extended Trend Log and set "Include in Reports" to True.  Ensure that the Log has correct Units
  2. Create a Meter Object inside the Energy Folder
  3. Change the Meter Trend Log to the appropriate Extended Trend Log.