Issue
Many sites use NAT for security purposes so question are asked if it is supported
Product Line
Andover Continuum, SmartStruxure Solution
Environment
Continuum
SmartStruxure
Bacnet
BBMD
NAT
Cause
There is a need to know if Continuum and/or SmartStruxure Bacnet support NAT
Resolution
We currently do not support NAT traversal in our BBMD implementations (Continuum or SmartStruxure). It is an optional feature we have not implemented. Request to add this feature should be directed to Product Marketing to include on the backlog for prioritization.
Related Continuum article: Lessons Learned Article #6943
Ashrae information: http://www.bacnet.org/Addenda/Add-135-2008o.pdf