Continuum Controller types and their model type numbers

Issue

Need the ability to identify controllers on a network and in a database

Product Line

Andover Continuum

Environment

Continuum

Infinet

Bacnet

Cause

Controllers have an internal model type number reference that can be used to identify which controller is in use on a system

Resolution

Here's a list of most of the Continuum controller types and their associated numbers

Controller List  - Click to download