RJ Modem Reference for the 9680

Issue

Modem commands for the internal modem for the 9680 are needed

Product Line

Andover Continuum

Environment

9680

RAS

Cause

Troubleshooting the modem in the 9680 may require knowledge of the Microtech modem and the commands

Resolution

The Netcontroller II Operation and Technical Guide references "RJ Modem AT Commands Reference" in order to customize the modem initialization string

Click her to download RJ Modem AT Commands Reference

There is no option for changing the DTMF frequency

Guide"