How to check the Bindings Diagnostics

Issue

Where can I check if all of the system bindings are configured without error?

Product Line

SmartStruxure Solution

Environment

Workstation Bindings Diagnostics.

V1.5.0 and above.

Cause

Validating the Bindings

Resolution

From the Workstation Control Panel, in the Engineering section select the "Bindings Diagnostics" link as per the following screenshot: