Issue
If multiple circuits are on a zone and only one circuit has a wink cycle on it, will all the circuits wink
Environment
I/NET site
Cause
If multiple circuits are on a zone and only one circuit has a wink cycle on it, will all the circuits wink
Resolution
No, the circuit with the wink cycle attached to it will be affected by the wink cycle. The other circuits will shut down when the zone goes to off.