Replacement part for RYB-922-11 repair kit

Issue

 RYB-922-11 is no longer available and needs to be replaced

Product Line

Field Devices

Environment

RYB-922-11

Repair Kit for VB-922x-0-4-11

Cause

repair kit no longer available

Resolution

There is no replacement for this kit. The customer will have to replace the valve body which probably will be the VB-7223-0-4-11 but verify which valve the customer has. Also since this new valve has a different stroke the customer will need to replace the actuator and linkage kit to ones that are used on the VB-7000 series valves.