Is it possible to manage the L-VIS screen with latex gloves?

Issue

Could the L-VIS screen be manage even if the operator is using latex gloves?

Product Line

TAC Vista, SmartStruxure Solution

Environment

Loytec L-VIS

Cause

The screen used on Loytec L-VIS is resistive, and due to that can be managed with latex gloves.

Resolution

The screen used on Loytec L-VIS is of resistive type, and due to that can be managed with latex gloves.