LonTalk adapter not working in VisiSat

Issue

No connection to Lon controllers from VisiSat

Product Line

Satchwell MicroNet

Environment

VisiSat

Windows 7

Cause

The Echelon Lon driver implementation in VisiSat does not support Windows 7. That means that if VisiSat is installed on Windows 7 (possible from version 2.1.185) it is not possible to use the Lon connection from VisiSat

Resolution

Install VisiSat on Windows XP to use the Lon connection