A PCS deploy fails and an error message comes up with the text Xif nnn could not be found

Issue

A PCS deploy fails and an error message comes up with the text "Xif nnn could not be found"

Product Line

SmartStruxure Solution

Environment

Project Configuration Server (PCS)

StruxureWare Building Operation 1.5 and newer

Cause

An import originating from a live system that has LON network containing network variables on the local node becomes a potential risk in PCS, but will import correctly as long as no local node variables are deleted. There is not currently support for dynamic update of changes on the local node in PCS.

Resolution

Leave an import containing Local Node variables unchanged, if importing to PCS