Failed to reload b3 controller

Issue

Failed to reload b3 controllers,The information for device commission detail indicates "the Object Identifier already existed".

Product Line

SmartStruxure Solution

Environment

Smart Struxure 1.50439

Automation Server

B3 field controllers

Cause

There are maybe some database inflict exist on AS.

Resolution

  1. Right Click AS and select "cold restart"
  2. Wait for AS go back online and try to reload b3 controllers, that maybe works.

   For unknown reason, the issue maybe come back again, but the solution can help you download the b3 controller smoothly at the moment and works well, and not impact the b3s' performance.