Untranslated infinity error when creating object in b3 device.

Issue

Untranslated infinity error when creating object in b3 device.

Product Line

SmartStruxure Solution

Environment

Workstation

b3

BACnet

Cause

b3 devices do not support certain characters in their objects name.

Resolution

b3 devices do not support certain characters in their objects name.

For example, creating an analog input using the name AI-1 will cause the error is the BACnet field is left blank, you can use the SBO name AI-1 but you will have to specify a name in the BACnet name field that is consistent with the b3 naming convention such as AI_1.